This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

RTOS/SENSOR-CONTROLLER-STUDIO: bug report, "Capacitive Touch example" project could not build with IAR if enable UART emulator(Sensor Controller Studio 2.4.0.793)

Expert 2560 points

Replies: 1

Views: 97

Part Number: SENSOR-CONTROLLER-STUDIO

Tool/software: TI-RTOS

The example Capacitive Touch with LaunchPad+ULP Sense BoosterPack have some issue build on IAR project.

Target chip select CC2652R1F,Revision select C(1.1),select proper UART RX/TX DIO.

Error[Pe136]: struct "<unnamed>#12" has no field "output" 

smile in the sunshine.

  • Guru 241570 points
    The title of the question indicate that you try to use the UART emulator together with cap sense?

    If that is the case, from the help description of the UART emulator:
    "This resource emulates a single full-duplex UART interface, which is useful when an additional system UART interface is needed. Once started, the UART emulator code runs continuously on the Sensor Controller until it is stopped. No other tasks can be run on the Sensor Controller during this time frame. "

    If not the case, please provide more details.

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.