Hey!
we're currently working on a simple CC2550 to CC2500 connection but have some problems to get it working reliably.
The CC2550 is transmitting with a constant datarate (2.4kbps/200kbps, doesn't matter), without exiting tx-mode (exit tx - start transmitting Preamble).
The CC2500 receiver is using an interrupt-based system with the same config as the CC2550 (as far as it makes sense).
Our symptoms are:
- RSSI close to the transmittet value
- PKTSTATUS register gets the Carrier-Sense=1, PQT_REACHED=1 (with different PQT-Configs) and CCA=0, so it sees that there is something transmitting on the channel. No Sync word-found flag is set.
Now we usually don't get any packages transmitted, but sometimes (without any pattern known (till now ;) ) packet transmission works fine.
What can be the reason for this?
Oscillator drift in the transmitter or receiver due to missing calibrations?
Register Config has been done with RFstudio, but we changed the datarate manually...
Thanks in advance,
Kai