This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C type LCD's supported by CC2530?

Other Parts Discussed in Thread: CC2530, CC2533, Z-STACK, CC2510

Hi, I'm planning to order cheap 16x2 LCD's that is run by the I2C serial protocol. I'm planning to use them as user interface for remote control purposes in a ZigBee environment. Unfortunately, as I saw in my CC2530's specs, I could not see an I2C supported serial interface.

Could the CC2530's 2 USART interfaces be converted into I2C interfaces? CC2530 has 2 USART I/F's that can be used as either UART or SPI mode. I actually could not see an I2C mode.

Is there a way maybe that these LCD's and USART interfaces can communicate with each other? I can see that they are run by the I2C protocol.

Thanks,

Jonathan