Other Parts Discussed in Thread: CC2520, CC2420, CC2500
Knowns anybody the (complex) impedance of the CC2520 chip? The datasheet only states the following:
"The RF input/output is high impedance and differential. When using an unbalanced antenna such as a monopole, a balun should be used in order to optimize performance. The balun can be implemented using low-cost discrete inductors and capacitors only or in combination with transmission lines replacing the discrete inductors."
Inductance values for transmission lines are not mentioned.
The microstrip balun in DN003, which is listed as application note for the CC2520 on its product page, is not the right one, because the CC2520 has no TXRX pin.
Information in the reference design (http://focus.ti.com/docs/toolsw/folders/print/cc2520em_refdes.html) only contains the layout files, no calculations, formulas or source files from the software it is designed in. This makes it very hard to develop a balun for boards with a different stackup or to choose a chip balun.
Thanks, Johan