Hi,
I have a full functional board with a trf7960 chip, now I have developed an upgrade of this board, and I would want to use 7979 instead of 7960A.
I have put the same circuitry of the 7960 board (for the rfid section) on this new one.
But if I put on it a 7970 chip I don't succedded in read the 7970 register via SPI with SS. I have seen that my command arrive to the miso e clk pin, but neither exit.
In the SAME board (phisically) I have put the 7960 and all work fine !
Please help me, I have just bougth 500 pcs. of 7970, and I must produce this 500 board next month.
Best regards and thanks in advance.
Marco