This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Design for CC1101 and CC1070 for 403 MHz?

Other Parts Discussed in Thread: CC1101, CC1070

I have both CC1101 and CC1070, and I want a very low power, short range (less than 10 m) transceiver system.

1) If I use CC1101, where can I find reference design and layout for 403MHz (I can find only for 433 and 868)?

2) If I use CC1070, which IC can I use as receiver IC that is compatible with it for 402 MHz (also I want refe5rence design for it for 402MHz) ?

If I start with CC1101 for 433MHz, how can I optimize it for 403MHz (any help appreciated) .

Thanks