Other Parts Discussed in Thread: CC2430, CC2520, MSP430F2618, CC1100, CC1101, CC2510, CC1100E, CC2500, CC2550
Hi, what are the difference between SmartRF04EB and SmartRF05EB? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
smartrf04eb
1)its based on outdated soc of ti know as cc2430(8051+RF)
2)it is only compatible with older zigbee stack zigbee-200)
3)obsolete
smartrf05eb
1)based on msp430f2618 controller and cc2520 high end RF
2)it can run latest zigbee pro stack
3)still active
---------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
---------------------------------------------------------------------------------------------------------
SmartRF04EB is active as well.
http://www.ti.com/tool/cc2510-cc2511dk, the CC2510-CC2511 Development Kit contains two SmartRF04 evaluation boards.
Hi Lei Chen1,
There are several differences between the two boards with regards to peripherals (LCD, breakout I/O, etc.).
The SmartRF04EB does not support newer LPRF SoCs and transceivers from Texas Instruments. It supports the following transceivers: CC1100, CC1100E, CC1101, CC2500, CC2550, and the following SoCs: CC1110/11, CC2510/11, CC2430.
Lei Chen1, if this didn't help, pelase as a more specific question, and I may be able to answer you better.
Br,
ABO
--
PS. Thank you for clicking Verify Answer below if this answered your question!