Other Parts Discussed in Thread: CC2500
We're working on a design using a MSP430 and CC2500. We are finding that the 2nd harmonic of the RF is present when the radio is in Rx mode. As a result we are not passing EN 300 440, or FCC 15.209. I've confirmed that the second harmic is being radiated from the board, and is not coming out the antenna. I've compared severalversions of our hardware, as well as a TI reference design, and all of them radiate the 2nd harmonic when in Rx mode. Has anyone else seen this 2nd harmonic problem?
Thanks,
Cory