This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 779
Hi All,
I have inherited an RF transmitter project which transmits a device ID as a UART, and I have been asked to develop a receiver to detect and display the ID.
The transmitter hardware is already designed and has been in manufacture for some time. It uses the TI CC1070 and is configured to transmit a burst of RF, encoded with the ID in UART mode at 9600 baud every 2 seconds. I have gone through the CC1070 datasheet and have re-written the device configuration table as follows:
rf_table retlw 0x81 ;00 MAIN [Select A, Normal operation, no power down, no reset] retlw 0x0A ;01 INTERFACE Internal Osc, PA_EN enabled and active high retlw 0x2D ;02 RESET Do not write '1's to this register retlw 0x00 ;03 ; ; MET 434.050 approx freq ; retlw 0x3A ;04 FREQ_2A } retlw 0x1F ;05 FREQ_1A ) FREQ=0x1D0F97, DITHER=1 retlw 0x2F ;06 FREQ_0A ) retlw 0x39 ;07 CLOCK_A REF_DIV=DIV2, MCLK_DIV1=DIV48, MCLK_DIV2=DIV2 ; retlw 0x3A ;08 FREQ_2B ) retlw 0x1F ;09 FREQ_2A ) FREQ=0x1D0F97, DITHER=1 retlw 0x2F ;0A FREQ_0B ) retlw 0x39 ;0B CLOCK_B REF_DIV=DIV2, MCLK_DIV1=DIV48, MCLK_DIV2=DIV2 ; retlw 0x44 ;0C VCO_CUR Both VCO_CURRENTs = 2.8mA retlw 0x03 ;0D MODEM UART mode, DCLK=1 retlw 0x9B ;0E DEVIATION TX_SHAPING=1, TXDEV_X=1, TXDEV_M=11 retlw 0x00 ;0F retlw 0x00 ;10 retlw 0x00 ;11 retlw 0x00 ;12 retlw 0x00 ;13 retlw 0x00 ;14 retlw 0x20 ;15 LOCK LOCK_SELECT=Cont, WINDOW_WIDTH=0, LOCK_MODE=0, LOCK_ACCURACY=0 retlw 0x00 ;16 retlw 0x07 ;17 ANALOG 402-470MHz band, PD_LONG=0, PA_BOOST=1, DIV_BUFF_CURRENT=3 retlw 0x04 ;18 BUFF_SWING PRE_SWING=0, TX_SWING=4 retlw 0x02 ;19 BUFF_CURRENT PRE_CURRENT=0, TX_CURRENT=2 retlw 0x93 ;1A PLL_BW PLL_BW=147 retlw 0x3C ;1B CALIBRATE CAL_START=0, CAL_DUE=0, CAL_WAIT=3, CAL_SELECT=1, CAL_ITERATE=4 retlw 0x0F ;1C PA_POWER PA_HIGH=0, PA_LOW=15 retlw 0x00 ;1D retlw 0x00 ;1E retlw 0x00 ;1F retlw 0x00 ;20 POWERDOWN All systems powered up
Using a handheld receiver, I can confirm that the transmitter is sending an RF burst every 2 seconds.
I have constructed a receiver using a microcontroller module connected to a cc1020mx module from a TI development kit, and have converted the -868MHz RF circuit to -433MHz, (values optimised for 434.050MHz using SmartRFStudio). I configure the CC1020 as follows:
// MAIN set by cc1020_reset spi_write(0x01, 0x0F); // INTERFACE int osc, DIO output, set PA and LNA control // RESET should be read only spi_write(0x03, 0x8F); // SEQUENCING PSEL power up, min RX_WAIT, max CS_WAIT spi_write(0x04, 0x3A); // FREQ_2A ) spi_write(0x05, 0x1F); // FREQ_1A ) FREQ = 0x1D0F97 spi_write(0x06, 0x2F); // FREQ_0A ) spi_write(0x07, 0x39); // CLOCK_A REF_DIV=DIV2, MCLK_DIV1=DIV48, MCLK_DIV2=DIV2 spi_write(0x08, 0x3A); // FREQ_2B ) spi_write(0x09, 0x1F); // FREQ_1B ) FREQ = 0x1D0F97 spi_write(0x0A, 0x2F); // FREQ_0B ) spi_write(0x0B, 0x39); // CLOCK_B REF_DIV=DIV2, MCLK_DIV1=DIV48, MCLK_DIV2=DIV2 spi_write(0x0C, 0x44); // VCO Both VCO_CURRENTs = 2.8mA spi_write(0x0D, 0x53); // MODEM ADC_DIV=DIV12, PN9 disabled, UART mode spi_write(0x0E, 0x9B); // DEVIATION TX_SHAPING=1, TXDEV_X=1, TXDEV_M=11 spi_write(0x0F, 0xC6); // AFC_CONTROL SETTLING=3, RXDEV_X=0, RXDEV_M=6 spi_write(0x10, 0x2F); // FILTER FILTER_BYPASS=0, DEC_SHIFT=1, DEC_DIV=DIV16 spi_write(0x11, 0x61); // VGA1 CS_SET=1, CS_RESET=1, VGA_WAIT=0, VGA_FREEZE=1 spi_write(0x12, 0x55); // VGA2 LNA2_MIN=0, LNA2_MAX=1, LNA2_SETTING=1, AGC_DISABLE=0, AGC_HYST=1, AGC_AVG=1 spi_write(0x13, 0x2F); // VGA3 VGA_DOWN=1, VGA_SETTING=31 spi_write(0x14, 0x2D); // VGA4 VGA_UP=1, CS_LEVEL=13 spi_write(0x15, 0x20); // LOCK LOCK_SELECT=Cont, WINDOW_WIDTH=0, LOCK_MODE=0, LOCK_ACCURACY=0 spi_write(0x16, 0x78); // FRONTEND LNAMIX_CURRENT=1, LNA_CURRENT=3, MIX_CURRENT=1, SDC_CURRENT=0, LNAMIX_BIAS=0 spi_write(0x17, 0x47); // ANALOG 402-470MHz band, LO_DC=1, VGA_BLANKING=0, PD_LONG=0, PA_BOOST=1, DIV_BUFF_CURRENT=3 spi_write(0x18, 0x14); // BUFF_SWING PRE_SWING=0, RX_SWING=2, TX_SWING=4 spi_write(0x19, 0x22); // BUFF_CURRENT PRE_CURRENT=0, RX_CURRENT=4, TX_CURRENT=2 spi_write(0x1A, 0xAF); // PLL_BW PLL_BW=175 spi_write(0x1B, 0x34); // CALIBRATE CAL_START=0, CAL_DUE=0, CAL_WAIT=3, CAL_ITERATE=4 spi_write(0x1C, 0x0F); // PA_POWER PA_HIGH=0, PA_LOW=15 spi_write(0x1D, 0x00); // MATCH RX_MATCH=0, TX_MATCH=0 spi_write(0x1E, 0x00); // PHASE_COMP PHASE_COMP=0 spi_write(0x1F, 0x00); // GAIN_COMP GAIN_COMP=0 spi_write(0x20, 0x00); // POWERDOWN All systems powered up
I call the initialisation routing and check for lock, (by reading the STATUS register (0x40)). STATUS returns not locked the first read after calibration, but thereafter returns 0xB2 or 0xB3, which seems to indicate it's locked successfully.
The image below shows the data sent to the DI pin of the CC1070 (top trace, yellow), and received at the DIO pin of the CC1020 (bottom trace, blue). As you can see, there is no discernible correlation between the data sent and the data received. Indeed, the received data looks like random bit transitions, as if the receiver is not receiving the transmitted signal.
I'm about out of ideas now, and RF is not my strong field. So if anyone has any suggestions, I'd really appreciate that. Many thanks in advance.
In reply to BillySugger:
In reply to Sverre:
Thank you Sverre, I don't have easy access to a spectrum analyser but I do have a tuned receiver. I can certainly make use of the methodical approach you suggest and if I can't validate the system elements without one, I'll have to hire an analyser. I appreciate your helpful advice in this.