Hi,
In our application we have to locate the NFC antenna (the inductor, actually) away of the PCB of the NFC IC
The NFC antenna will be cast inside distanced PCB with connectors at the end of the antenna conductors. then we plan to run a "rail" to the distanced PCB of the NFC IC, MCU etc. and connect to the PCB connectors-->matching components-->NFC IC.
Total distance between antenna and NFC IC 30-40cm. size of NFC antenna could be up to 10*5 cm or so.
my Q's are-
1. possible?
2. what would be the effective distance?
3. if possible, which lines should I use as rail between antenna PCB and main PCB?
attached sketch of the subject.
THX!
Ram