Hi,
I'm trying to get the DLP-RFID2 to write to an android phone (Nexus 5, and s7 edge for testing). Android uses the 14443A protocol, and everything works up until the SELECT command. I've tried the TRF7970EVM Control GUI and the same thing happens. No response after the SELECT command. Attached is my Salae capture when writing from my microcontroller. I'm following the steps in the TRF7970EVM User's Guide, so I'm guessing it might be the way Android NFC communicates? Any help would be greatly appreciated!