Hello support team,
I'm new to using CC430 with the EM430F6137RF900 board and programming them and so far I've got as far as testing the sample code RF_toggle_LED_Demo for the CC430 using CCSv6. The sample code provided was Fixed_GT_FIFO(Active_MHZ_868) and everything works, such as when I press the button it transmit and the other MCU receives. I was wondering how would I modify the code so that one of them continuously transmit without having to press a button and the other is always receiving? Also when its transmitting I'd like the Green LED to toggle so I know its transmitting and same for the Receiver when its receiving, the green LED will also toggle. Another thing is, when it is not receiving I'd like it to clear the green LED bit and turn on the Red LED. The sample code is provided below, thanks in advance.
#include "RF_Toggle_LED_Demo.h" extern RF_SETTINGS rfSettings; unsigned char packetReceived; unsigned char packetTransmit; unsigned char txBytesLeft = PACKET_LEN; // +1 for length byte unsigned char txPosition = 0; unsigned char rxBytesLeft = PACKET_LEN+2; // +2 for status bytes unsigned char rxPosition = 0; unsigned char lengthByteRead = 0; unsigned char RxBufferLength = 0; unsigned char TxBufferLength = 0; unsigned char * _p_Buffer = 0; unsigned char buttonPressed = 0; unsigned int i = 0; unsigned char transmitting = 0; unsigned char receiving = 0; unsigned char RxBuffer[PACKET_LEN+2] = {0}; unsigned char TxBuffer[PACKET_LEN]= { 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17, 0x18, 0x19, 0x20, 0x21, 0x22, 0x23, 0x24, 0x25, 0x26, 0x27, 0x28, 0x29, 0x30, 0x31, 0x32, 0x33, 0x34, 0x35, 0x36, 0x37, 0x38, 0x39, 0x40, 0x41, 0x42, 0x43, 0x44, 0x45, 0x46, 0x47, 0x48, 0x49, 0x50, 0x51, 0x52, 0x53, 0x54, 0x55, 0x56, 0x57, 0x58, 0x59, 0x60, 0x61, 0x62, 0x63, 0x64, 0x65, 0x66, 0x67, 0x68, 0x69, 0x70, 0x71, 0x72, 0x73, 0x74, 0x75, 0x76, 0x77, 0x78, 0x79, 0x80, 0x81, 0x82, 0x83, 0x84, 0x85, 0x86, 0x87, 0x88, 0x89, 0x90, 0x91, 0x92, 0x93, 0x94, 0x95, 0x96, 0x97, 0x98, 0x99, }; void main( void ) { // Stop watchdog timer to prevent time out reset WDTCTL = WDTPW + WDTHOLD; // Increase PMMCOREV level to 2 for proper radio operation SetVCore(2); ResetRadioCore(); InitButtonLeds(); InitTimer(); // Clean out the RX Buffer rxPosition = PACKET_LEN+2; while(rxPosition--) { RxBuffer[rxPosition] = 0; } InitRadio(); ReceiveOn(); while (1) { P1IE |= BIT7; // Enable button interrupt __bis_SR_register( LPM3_bits + GIE ); __no_operation(); if (buttonPressed) // Process a button press->transmit { ReceiveOff(); // Button means TX, stop RX receiving = 0; TransmitPacket(); buttonPressed = 0; // Re-enable button press } if(receiving) { ReceivePacket(); __no_operation(); } if(!transmitting) { ReceiveOn(); } } } void ReceivePacket(void) { rxBytesLeft = PACKET_LEN + 2;// Set maximum packet leng + 2 for appended bytes rxPosition = 0; packetReceived = 0; __delay_cycles(2800); // Wait for bytes to fill in RX FIFO TA0CCR1 = RX_TIMER_PERIOD; // x cycles * 1/32768 = y us TA0CCTL1 |= CCIE; TA0CTL |= MC_2 + TACLR; // Start the timer- continuous mode __bis_SR_register(LPM3_bits + GIE); __no_operation(); TA0CCR1 = RX_TIMER_PERIOD; TA0CCTL1 &= ~(CCIE); TA0CTL &= ~(MC_3); // Turn off timer __no_operation(); } void TransmitPacket(void) { //P3OUT |= BIT6; // Pulse LED during Transmit P1OUT |= BIT0; txBytesLeft = PACKET_LEN; txPosition = 0; packetTransmit = 0; transmitting = 1; Strobe( RF_STX ); // Strobe STX TA0CCR1 = TX_TIMER_PERIOD; // x cycles * 1/32768 = y us TA0CCTL1 |= CCIE; TA0CTL |= MC_2 + TACLR; // Start the timer- continuous mode __bis_SR_register(LPM3_bits + GIE); __no_operation(); TA0CCR1 = TX_TIMER_PERIOD; // x cycles * 1/32768 = y us TA0CCTL1 &= ~(CCIE); TA0CTL &= ~(MC_3); // Turn off timer // P3OUT &= ~BIT6; // Turn off LED after Transmit P1OUT &= ~BIT0; } void ReceiveOn(void) { RF1AIES &= ~BIT9; RF1AIFG = 0; // Clear pending RFIFG interrupts RF1AIE |= BIT9; // Enable the sync word received interrupt // Radio is in IDLE following a TX, so strobe SRX to enter Receive Mode Strobe( RF_SRX ); __no_operation(); } void ReceiveOff(void) { RF1AIE &= ~BIT9; // Disable RX interrupts RF1AIFG &= ~BIT9; // Clear pending IFG RF1AIES &= ~BIT9; // Switch back to to sync word // It is possible that ReceiveOff is called while radio is receiving a packet. // Therefore, it is necessary to flush the RX FIFO after issuing IDLE strobe // such that the RXFIFO is empty prior to receiving a packet. Strobe(RF_SIDLE); Strobe(RF_SFRX); } //------------------------------------------------------------------------------ // void pktRxHandler(void) // // DESCRIPTION: // This function is called every time a timer interrupt occurs. The // function starts by retreiving the status byte. Every time the status // byte indicates that there are available bytes in the RX FIFO, bytes are // read from the RX FIFO and written to RxBuffer. This is done until the // whole packet is received. If the status byte indicates that there has // been an RX FIFO overflow the RX FIFO is flushed. Please see the // EM430F6137RF900 RF Examples User Manual for a flow chart describing this // function. //------------------------------------------------------------------------------ void pktRxHandler(void) { unsigned char RxStatus; unsigned char bytesInFifo; // Which state? RxStatus = Strobe(RF_SNOP); switch(RxStatus & CC430_STATE_MASK) { case CC430_STATE_RX: // If there's anything in the RX FIFO.... if (bytesInFifo = MIN(rxBytesLeft, RxStatus & CC430_FIFO_BYTES_AVAILABLE_MASK)) { // Update how many bytes are left to be received rxBytesLeft -= bytesInFifo; // Read from RX FIFO and store the data in rxBuffer while (bytesInFifo--) { RxBuffer[rxPosition] = ReadSingleReg(RXFIFO); rxPosition++; } if (!rxBytesLeft){ packetReceived = 1; receiving = 0; lengthByteRead = 0; ReceiveOff(); P1OUT ^= BIT0; // Toggle LED1 } } break; default: if(!packetReceived) { packetReceived = 1; } rxBytesLeft = 0; receiving = 0; ReceiveOff(); break; } } // pktRxHandler //------------------------------------------------------------------------------ // void pktTxHandler(void) // // DESCRIPTION: // This function is called every time a timer interrupt occurs. The function starts // by getting the status byte. Every time the status byte indicates that there // is free space in the TX FIFO, bytes are taken from txBuffer and written to // the TX FIFO until the whole packet is written or the TXFIFO has underflowed. // See the EM430F6137RF900 RF Examples User Manual for a flow chart describing // this function. //------------------------------------------------------------------------------ void pktTxHandler(void) { unsigned char freeSpaceInFifo; unsigned char TxStatus; // Which state? TxStatus = Strobe(RF_SNOP); switch (TxStatus & CC430_STATE_MASK) { case CC430_STATE_TX: // If there's anything to transfer.. if (freeSpaceInFifo = MIN(txBytesLeft, TxStatus & CC430_FIFO_BYTES_AVAILABLE_MASK)) { txBytesLeft -= freeSpaceInFifo; while(freeSpaceInFifo--) { WriteSingleReg(TXFIFO, TxBuffer[txPosition]); txPosition++; } if(!txBytesLeft) { RF1AIES |= BIT9; // End-of-packet TX interrupt RF1AIFG &= ~BIT9; // clear RFIFG9 while(!(RF1AIFG & BIT9)); // poll RFIFG9 for TX end-of-packet RF1AIES &= ~BIT9; // End-of-packet TX interrupt RF1AIFG &= ~BIT9; // clear RFIFG9 transmitting = 0; packetTransmit = 1; } } break; case CC430_STATE_TX_UNDERFLOW: Strobe(RF_SFTX); // Flush the TX FIFO __no_operation(); // No break here! default: if(!packetTransmit) packetTransmit = 1; if (transmitting) { if ((TxStatus & CC430_STATE_MASK) == CC430_STATE_IDLE) { transmitting = 0; } } break; } } // pktTxHandler void InitTimer(void) { P5SEL |= 0x03; // Set xtal pins LFXT_Start(XT1DRIVE_0); TA0CCR1 = RX_TIMER_PERIOD; // x cycles * 1/32768 = y us TA0CCTL1 = CCIE; // Enable interrupts TA0CTL = TASSEL__ACLK + TACLR; // ACLK source } void InitButtonLeds(void) { // Set up the button as interruptible P1DIR &= ~BIT7; P1REN |= BIT7; P1IES &= BIT7; P1IFG = 0; P1OUT |= BIT7; P1IE |= BIT7; // Initialize Port J PJOUT = 0x00; PJDIR = 0xFF; // Set up LEDs P1OUT &= ~BIT0; P1DIR |= BIT0; P3OUT &= ~BIT6; P3DIR |= BIT6; } void InitRadio(void) { // Set the High-Power Mode Request Enable bit so LPM3 can be entered // with active radio enabled PMMCTL0_H = 0xA5; PMMCTL0_L |= PMMHPMRE_L; PMMCTL0_H = 0x00; WriteRfSettings(&rfSettings); WriteSinglePATable(PATABLE_VAL); } /************************************** * Interrupt Service Routines **************************************/ #pragma vector=TIMER0_A1_VECTOR __interrupt void TIMER0_A1_ISR(void) { switch(__even_in_range(TA0IV,14)) { case 0: break; case 2: if(receiving) { TA0CCR1 += RX_TIMER_PERIOD; // 16 cycles * 1/32768 = ~500 us pktRxHandler(); if(packetReceived) __bic_SR_register_on_exit(LPM3_bits); } else if(transmitting) { TA0CCR1 += TX_TIMER_PERIOD; // 16 cycles * 1/32768 = ~500 us pktTxHandler(); if(packetTransmit) __bic_SR_register_on_exit(LPM3_bits); } break; case 4: break; // CCR2 not used case 6: break; // Reserved not used case 8: break; // Reserved not used case 10: break; // Reserved not used case 12: break; // Reserved not used case 14: break; // Overflow not used } } #pragma vector=CC1101_VECTOR __interrupt void CC1101_ISR(void) { switch(__even_in_range(RF1AIV,32)) // Prioritizing Radio Core Interrupt { case 0: break; // No RF core interrupt pending case 2: break; // RFIFG0 case 4: break; // RFIFG1 case 6: break; // RFIFG2 case 8: break; // RFIFG3 case 10: break; // RFIFG4 case 12: break; // RFIFG5 case 14: break; // RFIFG6 case 16: break; // RFIFG7 case 18: break; // RFIFG8 case 20: // RFIFG9 if(!(RF1AIES & BIT9)) // RX sync word received { receiving = 1; __bic_SR_register_on_exit(LPM3_bits); // Exit active } else while(1); // trap break; case 22: break; // RFIFG10 case 24: break; // RFIFG11 case 26: break; // RFIFG12 case 28: break; // RFIFG13 case 30: break; // RFIFG14 case 32: break; // RFIFG15 } } #pragma vector=PORT1_VECTOR __interrupt void PORT1_ISR(void) { switch(__even_in_range(P1IV, 16)) { case 0: break; case 2: break; // P1.0 IFG case 4: break; // P1.1 IFG case 6: break; // P1.2 IFG case 8: break; // P1.3 IFG case 10: break; // P1.4 IFG case 12: break; // P1.5 IFG case 14: break; // P1.6 IFG case 16: // P1.7 IFG __delay_cycles(1000); // debounce delay buttonPressed = 1; P1IE = 0; // Debounce by disabling buttons P1IFG = 0; __bic_SR_register_on_exit(LPM3_bits); // Exit active break; } }