Hello
I unpacked for the first time a cc-debugger that is on my shelf for several years.
Plugged it in my win7 64 bits. It is recognized by windows and smartRF studio 7. I clicked on "show connected devices".
Software aked me to upgrade from version (as far as I remember ) 22 to 44. I answered NO.
It worked pretty well. I was able to see the received frames.
I closed everything an re-opened smartRF , removed the connected CC2530 and answered YES to the
upgrade dialog. Upgrade seems ok.
I clicked on "show connected devices". software asked me to upgrade from version 0 to 44 (!!)
I answered YES and upgrade seems ok.
I disconnected cc debugger from pc, now it is not recognized anymore by windows. I installed the
driver swrc212a but it's not better.
What can I do?
Thanks
Julien