Other Parts Discussed in Thread: TMS3705, , UCC27424, MSP430F6659, MSP430FR5739
,Hi,
I'm working on a design with TMS3705 and TMS37157.
The transmitter hardware with the TMS3705 is ready and needs to be programmed to do the job.
The transponder is on prototype level at the moment.
To code the software for the TMS3705, I need to understand how the communication between TMS3705 and TMS37157 works.
For this I use the eZ430-TMS37157 development tool.
The communication of the TMS3705 looks like this at the moment:
The blue line is TXCT, the red is SCIO, the green is the field (external sensor), the orange is the SENSE input of the TMS3705.
According to the datasheet of the TMS37157 it sends the answers via an FSK (134.7 and 123.7 kHz)
My question is, the TMS37157 is responding (red line second bit sequence), but I can't see the FSK response in the field or the SENSE input.
Where is it?
Kind regards
Gerd