Other Parts Discussed in Thread: CC1101
Hello Experts,
We are evaluating CC2500 on MSK 500kbps by using SmartRF studio and EM. Other than below parameters, we are using the default register settings of SmartRF studio 7.
1. Changing MDMCFG2.SYNC_MODE shows below PER
0x71 : PER 100%( all failed)
0x72 : PER 15%
0x73 : PER 0% ( all good)
Why does sync word length affect PER? We want to use 16 bit sync word if possible.
2. When should we use MDMCFG2.SYNC_MODE with larger than b'101 (15/16 + carrier sense above threshold)?
3. How to use PKTCTRL1.PQT?
When setting PKTCTRL1.PQT to 3, PER described on above 1 shows almost 0% ( good result)
Best Regards,
Uchikoshi