Hello,
I am working on a project where I would like to use a "powerless" RF board connected to an ECG sensor and I have observed that I can only have a distance of less then 10 cm using energy harvesting between the "voltage sender" and the RF430FRL152HEVM. I was wondering if I would be able to increase this distance by slowly charging up a capacitor and then using the capacitor to power the RF430FRL152HEVM which will then power my ECG sensor.