Part Number: RF430FRL152H
Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
Hello,
I was trying to upload some code onto the RF430FRL152H chip, using the MSP-FET430UIF, and the L092 Active Cable. CCS gives the error, "MSP430: Error connecting to the target: Unknown device".
I have made the following connections:
L092 Active Cable (10 pin side) | RF430FRL152H
PIN 10 (ULVRST) | PIN 10 (RESET)
PIN 9 (GND) | PIN 25 (GND)
PIN 8 (THOLD) ---> NOT CONNECTED
PIN 7 (ULKTCK) | PIN 22 (TCK)
PIN 6 ---> NOT CONNECTED
PIN 5 (ULVTMS) | PIN 19 (TMS)
PIN 4 (GND) | PIN 25 (GND)
PIN 3 (ULVTDI) | PIN 21 (TDI)
PIN 2 (VCCULV) | PIN 3 (VDDSW)
PIN 1 ( ULVTDO) | PIN 20 (TDO)
Is this correct?
Best,
Mehzabin