Hi,
Because of the low success rate of trust, we are now testing with CC2510DK.
But the same register settings have different results.(OK => NG) Why?Pls help.
(Tx,Rx,as same)
(OK↓)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Because of the low success rate of trust, we are now testing with CC2510DK.
But the same register settings have different results.(OK => NG) Why?Pls help.
(Tx,Rx,as same)
(OK↓)
Hi, R.M
At the beginning, the company developed products and found that the rate dropped from 42K to 41K.
The success rate of reception will drop.
It will completely fail at 39K.
Now it is tested with CC2510DK.
Now I'm using CC2510DK on the Tx and Rx side.
Will fill in the 42K parameters into Smartrf Studio 7. Test OK.
After dropping 42K to 39K, test NG.
Then adjust the 42K parameters and test NG.
Probably this is the case.
<?xml version="1.0" encoding="ISO-8859-1"?> <!DOCTYPE configuration SYSTEM "C:/Program Files (x86)/Texas Instruments/SmartRF Tools/SmartRF Studio 7/config/xml/configdata.dtd"[]> <dcpanelconfiguration> <Devicename>CC2510</Devicename> <Description>Saved configuration data</Description> <registersettings> <Register> <Name>AGCCTRL0</Name> <Value>0xb0</Value> </Register> <Register> <Name>AGCCTRL1</Name> <Value>0x10</Value> </Register> <Register> <Name>AGCCTRL2</Name> <Value>0xc7</Value> </Register> <Register> <Name>BSCFG</Name> <Value>0x1c</Value> </Register> <Register> <Name>DEVIATN</Name> <Value>0x44</Value> </Register> <Register> <Name>FOCCFG</Name> <Value>0x1d</Value> </Register> <Register> <Name>FREND1</Name> <Value>0xb6</Value> </Register> <Register> <Name>FREQ0</Name> <Value>0x4e</Value> </Register> <Register> <Name>FREQ1</Name> <Value>0x6c</Value> </Register> <Register> <Name>FREQ2</Name> <Value>0x5c</Value> </Register> <Register> <Name>FSCAL0</Name> <Value>0x66a5</Value> </Register> <Register> <Name>FSCAL1</Name> <Value>0x66a5</Value> </Register> <Register> <Name>FSCAL2</Name> <Value>0x66a5</Value> </Register> <Register> <Name>FSCAL3</Name> <Value>0x66a5</Value> </Register> <Register> <Name>FSCTRL1</Name> <Value>0x08</Value> </Register> <Register> <Name>IOCFG0</Name> <Value>0x32</Value> </Register> <Register> <Name>IOCFG2</Name> <Value>0x06</Value> </Register> <Register> <Name>LQI</Name> <Value>0x7f</Value> </Register> <Register> <Name>MCSM1</Name> <Value>0x10</Value> </Register> <Register> <Name>MDMCFG0</Name> <Value>0x7a</Value> </Register> <Register> <Name>MDMCFG1</Name> <Value>0x02</Value> </Register> <Register> <Name>MDMCFG2</Name> <Value>0x83</Value> </Register> <Register> <Name>MDMCFG3</Name> <Value>0x19</Value> </Register> <Register> <Name>MDMCFG4</Name> <Value>0x7b</Value> </Register> <Register> <Name>PA_TABLE0</Name> <Value>0xfe</Value> </Register> <Register> <Name>PKTCTRL0</Name> <Value>0x05</Value> </Register> <Register> <Name>TEST0</Name> <Value>0x09</Value> </Register> <Register> <Name>TEST1</Name> <Value>0x31</Value> </Register> </registersettings> <dcpanel> <Property role="44" name="m_chkRegView">2</Property> <Property role="44" name="m_chkRfParameters">2</Property> <Property role="37" name="m_tabUserMode">1</Property> <Property role="33" name="m_easyModeSettings">-1</Property> <Property role="33" name="m_typicalSettings">-1</Property> <Property role="37" name="m_testFuncPanel">3</Property> </dcpanel> <rfparameters> <Property role="46" name="Xtal frequency">26.000000</Property> </rfparameters> <conttx> <Property role="45" name="m_rbtModulated">1</Property> <Property role="45" name="m_rbtUnmodulated">0</Property> <Property role="46" name="m_cmbDataFormat">-1</Property> <Property role="44" name="m_chkFreqSweep">0</Property> <Property role="44" name="m_chkChanSweep">0</Property> </conttx> <contrx> <Property role="46" name="m_cmbDataFormat">-1</Property> <Property role="44" name="m_chkAutoScroll">2</Property> </contrx> <packettx> <Property role="42" name="m_edtPayloadSize">30</Property> <Property role="42" name="m_edtPacketCount">100</Property> <Property role="42" name="m_edtPacketCountEsy">100</Property> <Property role="42" name="m_edtRandomPacketData">29 23 be 84 e1 6c d6 ae 52 90 49 f1 f1 bb e9 eb b3 a6 db 3c 87 0c 3e 99 24 5e 0d 1c </Property> <Property role="42" name="m_edtPacketData"></Property> <Property role="42" name="m_edtAccessAddress"></Property> <Property role="44" name="m_chkAddSeqNbr">2</Property> <Property role="44" name="m_chkInfinite">0</Property> <Property role="44" name="m_chkInfiniteEsy">0</Property> <Property role="45" name="m_rbtRandom">1</Property> <Property role="45" name="m_rbtText">0</Property> <Property role="45" name="m_rbtHex">0</Property> <Property role="44" name="m_chkAdvanced">0</Property> </packettx> <packetrx> <Property role="42" name="m_edtPacketCount">100</Property> <Property role="42" name="m_edtPacketCountEsy">100</Property> <Property role="42" name="m_edtAccessAddress"></Property> <Property role="44" name="m_chkInfinite">0</Property> <Property role="44" name="m_chkInfiniteEsy">0</Property> <Property role="46" name="m_cmbViewFormat">0</Property> <Property role="44" name="m_chkSeqNbrIncluded">2</Property> <Property role="42" name="m_edtDumpFile"></Property> <Property role="44" name="m_chkAdvanced">0</Property> </packetrx> <commandpanel> <Property role="44" name="m_chkInsertLength">0</Property> <Property role="42" name="m_edtTxFifo"></Property> <Property role="42" name="m_edtRxFifo"></Property> <Property role="46" name="m_cmbInstrInput">-1</Property> </commandpanel> </dcpanelconfiguration>