Other Parts Discussed in Thread: MSP-FET,
Hello,
I buy the RF430-TMPSNS-EVM, EXP7970ABP and EXP430g2ET. At first, the distance between the RF430-TMPSNS-EVM and EXP7970ABP is about 5cm. However, my project is to enlarge the distance to 1m. So I want to programming the RF430TMPSNSEVM and connect the additional power source. Now the first question is that which pin I need to connect when I want to programming the device? Second one is that should I need a debug tool when I programming it?
The last question is that is this tag has semi-passive function?