This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 8
Views: 370
Part Number: CC2544
Hi,
My customer is looking for the TI CC2544 USB CDC Driver and they also want to know if it pass Microsoft WHQL certification.
Thanks.
Hi Mike,
The USB CDC driver is included with the TI BLE Stack for example, so one way to get this is to download and install the USB Stack for CC254x.
I do not know whether or not it pass MS WHQL certification.
Regards,Fredrik
Hector and Fredrik,
I will pass these message on to my customer and check if they have any other questions.
Thanks for your help.
Mike Wu
In reply to Mike Wu1:
Disregard my previous post, I mentioned the wrong drivers which don't have anything to do with the CDC drivers.
In reply to Hector_r:
Hi Hector,
Got it and still thanks for your help.
my customer met the following error while running WHQL test for TI CC2544 USB CDC driver:
InfVerif failed for Driver. Partial Log:Error 1203 in ccxxxx_usb_cdc.inf, line 49 : Section [fakemodemcopyfilesection] not found.
The ccxxxx_usb_cdc.inf in BLE-CC254x-1.5.0.16 is attached, please help to provide comments.
ccxxxx_usb_cdc.7z
I am not sure what this means. What are your customer trying to do?
In reply to Fredrik K:
USB Test-CC2544.docx
Hi Fredrik,
My customer is using TI CC2544 and can not pass the WHQL test of Microsoft Win7.
The Error message of WHQL test of Microsoft Win7 is :
PS. The ccxxxx_usb_cdc.inf is from BLE-CC254x-1.5.0.16
Please help to check if TI can provide some suggestion for the error message.
Doing some searching on this online, this seem to be a common issue for these kinds of drivers when moving to newer windows version. Take this for example:
https://social.msdn.microsoft.com/Forums/windowsdesktop/en-US/0d1632e9-8e24-4ecf-a58c-edf0ad4496dd/fakemodemcopyfilesection-not-defined?forum=whck
Not sure this is something we can help out with, I can verify that adding the empty section will make the error go away but I can't comment on if this impacts the functionality of the device in any way. The customer would have to setup their driver and test it out, I would assume they still have to create their own inf file for the end product in the end.
Best regards,
M-W