This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 120
Part Number: CC2544
Hi,
The datasheet of CC2544 mention "Extensive Baseband Automation, Including Auto-Acknowledgement and Address decoding."
My customer want to know more about the "Auto-Acknowledgement ".
Is it means Auto-Acknowledgement for I2C bus , not Proprietary 2.4GHz communication ?
Mike
Hi Mike,
Auto-ack is for the RF communication. You will find more details in the CC2543/CC2544/CC2545 User´s Guide.
Regards,Fredrik
In reply to Fredrik K:
Hi Fredrik,
Thanks for your feedback and the feedback is passed on to my customer.
Please help to advice if there exist TI Software Examples of CC2543/CC2544 which can help my customer to develop a frequency-jump mechanism for building a robust Proprietary 2.4GHz communication.
Thanks.
In reply to Mike Wu1:
For the CC2544 we only have a simple RF example, the PER test.
If they need a more robust solution, they must either develop it themselves, or select another device which is supported by a defined protocol.