Hi team,
can you help my customer with the following inquiry?
"I'm trying to run BeagleBoneBlack with the Wireless Connectivity Cape (element14).
I got stuck during the installation of the SDK on my beagle bone black:
First I installed a Virtual Box with Linux 18.4 and then downloaded the binary for the palform AM335X in the Virtual Box: ti-processor-sdk-linux-am335x-evm-06.00.00.07-Linux-x86-Install.bin
I also executed the binary, and next I need to get Beagle Bone Black to boot not from eMMC, but from the SD card.
The problem is, I have different suggestions in software-dl.ti.com/.../Overview.html :
1.2 Building the SDK ---> there are steps how to prepare the environment in Linux Host to build the layers of yocto project.
But I'm not sure if this is necessary to test the cape? Finally I made the cape run with a normal Debian.
1.1.5 Run Setup Scripts --> here you have to make sure that BBB is not booted by the eMMC. Would you have a more recent introduction for this step, because the paths or file names are now different.
6.1.12. Ubuntu 14.04 Set Up to Network Boot an AM335x/AM437x Based Platform ---> This step allows you to leave the development environment on the host and boot from there.
All in all I am uncertain which steps I have to follow. The cape doesn't work if BBB is booted from the eMMC, so BBB must boot from SD card, but there are instructions in "Getting Started" that do exactly the opposite."
Thank you,
Franz