Part Number: LAUNCHXL-CC1352P
I opened the SmartRF Flash Programmer in order to flash program my image to the CC1352 on board the CC1352P1 launchpad , which is connected with a USB cable to my PC. once choosing the XDS110 from the connected devices pane (left side) i was asked to perform an update to the XDS110. I pressed ok and after a few seconds the update stopped on 50% and said theres some kind of ERROR(dont remember which, and its already not availble for me). I waited a bit more and since there was no change I pressed cancel. Then after resetting the launchpad, the XDS drivers didnt load anymore and the device manager doesnt show any xds device under "Ports".
It seems the firmware upgrader messed up the xds firmware and it doesnt load anymore..my launch pad is useless now..@!