Other Parts Discussed in Thread: TRF7960A
Hi!
We have single board with design similar to reference design, matching circuit is with custom values. Application is for RFID ISO14443a. On some occasions individual boards are having poor sensitivity like issues. TRF7970A FIFO is padded with 0x00 zeros when tag is located at normal reading distance which is about inch from the PCB. Extra bytes are always 0x00. Some of the tag bytes may be found from the start of the FIFO buffer and reading fails due to wrong ID. It's random if it's read correctly or is it padded with variable number of extra bytes. At very close distance usually working just fine. TX power is set high in Chip Status Control register.
Issue is found from about 1% of the boards and started on spring 2019. No problems faced before this.
I think the problem is self-jamming where TX signal is leaking to RX side at too high level, but have no proof. This might be due to component value variation if something is at the very edge.
Any suggestions from where to start?