This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2500: CC2500 QUESTIONS

Part Number: CC2500

Hi 

I have a few questions about the CC2500 IC. 

  • How many CC2500 can i connect to each other? 
  • Does it have a paring method (like bluetooth), or just plug and transmit data to other CC2500?
  • Is it a full duplex or half duplex connection between two CC2500?

Thanks for answering

Jose

    • How many CC2500 can i connect to each other? 
      • CC2500 is a transceiver that just implement the physical layer in a protocol. How many devices you can connect together will depend on the protocol.  
    • Does it have a paring method (like bluetooth), or just plug and transmit data to other CC2500?
      • CC2500 is a transceiver that just implement the physical layer in a protocol. How a CC2500 should join a network etc is dependent on how you write ypur software.

    • Is it a full duplex or half duplex connection between two CC2500?
      • Half duplex