I am using the RF430FRL154H in a very compact design, and I would like to use fewer capacitors than that in the application circuit in the datasheet. It shows capacitors on VDDSW, VDD, VDDH, VDDB, VDD2X SVSS, and RST as well as the flyback capacitor on CP1 and CP2. I am only using the VDDH supply external to the chip. Which capacitors should I populate, and which are optional?
It would seem as though VDD, VDDSW, VDDB, VDD2X, and SVSS caps are all not necessary for my application. However, I noticed when I removed a cap from VDDSW/VDDB, the tag stopped responding.