Other Parts Discussed in Thread: MSP430F2370
Hi,
I am working on TRF7970A EVM with DM0 Mifare classic sample application. By reading the TRF7970A datasheet, what I understand is, VDD_X will be generated only when (EN=0 & EN2=1) or (EN=1 & EN2=X) but not when (EN=0 & EN2=0).
In the TRF7970A EVM, the EN2 is connected to GND and EN is controlled by MSP430F2370. When the TRF7970A EVM is connected to the USB port, VIN is available and (EN=0 & EN2=0). After 2ms delay from VIN, the VDD_X regulated supply is generated. However, the EN and EN2 are still LOW. I could see that SYS_CLK is generated only when EN=1. Please refer the below image.
I could not understand how the VDD_X regulated supply is generated and the MSP430 is powered ON while (EN=0 & EN2=0) when the TRF7970A EVM is connected to the USB port.
Can anyone explain this please?
Thanks and Regards,
Sunil