Other Parts Discussed in Thread: CC1101
Greetings,
our company is developing a couple of products based respectively on
cc1111 and cc1101 chips.
At the moment we need to run EMI and Radio compatibility certification tests for ETSI.
Applicable norms are EN 300-220, EN 301-489-3.
Our application works with the following settings:
- +10 dB Radio power
- 250KBaud/s speed
-868.0-868.6 band
-GFSK modulation
We followed the reference design from ezChronos for the cc1111 based product and TI reference designs for antenna pcb for cc1101.
During the EMC radiated emission tests we found out the following
non-conformities:
For both cc1111 and cc1101:
Several over-the-limit emission peaks in the frequency bands adjacent to the 868.0-868.6 band.
For cc1101 only
Some spurious emission at 816.36, 764.52, 712, 660.12 .... (probably due to our layout)
Apparently the first of the two is due to the large emission envelope that spans far beyond the usable band (868.0-868.6). (Please see attached documents)
CC1101 setted with +10dBm output power, 250Kbps.

CC111 large emission envelop
Do you have any suggestion where I can try to fix in order to solve this issue?
BR,
Giordano