Hi
I'm in the process of developing production/testing equipment for a cc2540 BLE product.
I'm planing on using the cc-debugger for flashing the firmware but there is one bottleneck I want to come around.
If the testrigg is powered up before a board is attached to it the CC-Debugger will shine red and when a board is
attached it wont flash it until the reset button on the CC-Debugger is pressed and the led shines green.
Is there a way to initiate this reset from software, I'm using the SmartRFProgConsole tool.
Or will I have to add an external relay to toggle this button?
Best Regards
Joakim Arnsby