Hi.
Problem has come out with a pair of ring CC2530 RF4CE.
Pairing is released after pairing, repeating the ON / OFF the power by using the remote control.
Repeat 100 times, the number of power ON / OFF occurs at a frequency of once or twice.
Software you are using, and are based on the RemoTI.
Point of order to solve the problem, to be worried about something or will not there?
In addition, when the state of the above is happening, ROM of internal or CC2530 will be considered What kind of state?
Am sorry to have caused trouble, but would appreciate the help.
Best Regards,
hamada