This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Powerless RF transmitter for finding underground objects

Other Parts Discussed in Thread: TMS37157, RI-STU-MRD2

Sir

        Is there any RF IC/Component which transmit RF signal without any battery power. My application is to locate an object buried under earth. Suppose in Optical fiber cables (OFC) joints are duried under earth about 1.5m depth from ground level. my project is to locate this joint kits. but the joint kits are plastic objects so it is not possible to locate with cheeper devices. So I want to put some RF transmitting device inside joint kits during closing the earth so that I could locate the joint by using some RF sensor from the ground itself.

          So for this project RF IC/Component should work without power or this IC/Component should work from outside RF energy while checking. And the RF IC/Component using inside joint kite should be cheaper because we have to use it in lakh's of joint kits all over the OFC network.

           So please suggest an RF IC/Component and/or method for doing this project

thanking you

Prasanth