Other Parts Discussed in Thread: CC1101
Hello,
I'm designing a product using the CC1101 transceiver.
I can currently receive at a range of about 60 meters. I need to push this up a bit.
I was thinking that if I enable the FEC/Interleaver, the range would increase, however
it turned out it would actually decrease. Same thing if I turn down the baudrate.
Would this indicate that the crystals are not enough accurate enough?
I have a log of the received data of a typical message with and without FEC, as well as the parameter settings,
visible in the screenshots here: edab.nu/flextag. The start and end of a message is shown with the cursor markers.