Other Parts Discussed in Thread: TRF4140-Q1
We are about to design our first base station for HDX animal tags based on the TMS3705.
We plan to make it as a research / development platform for our application, with an aim to get as long reading range as possible with our antenna being limited in size.
One of the optional circuit we are planning to include there is an additional RF amplifier with an active band-pass filter with the centre frequency of (around (134.2 + 123.2) / 2 =) 128.7 kHz to increase receiver sensitivity.
My attempts to prototype it on the breadboard and to hook it up to the RI-ACC-ADR2-10 have not been successful so far, as I am getting a lot of "false positive" readings out of TMS3705. I presume that this is due to the TMS3705 receiver picking background noise from the connecting wires.
To avoid further efforts, may I ask you please for your professional opinion: do you think that TMS3705 receiver is as sensitive as it can get in practice or adding an extra pre-amplifier could improve the overall system sensitivity (and, therefore, the reading range)?