If my Vin (pin2) is 3.3V, what is the maximum output voltage that can be achieved on the Vdd_x output (pin 32) with the appropriate register setting?
Table 6-2 in the datasheet states the various register settings for various output voltage values of Vdd_x, specifically for the 3V system. However, it has a register setting for a Vdd_x value of 3.4V. However I don't believe that the internal regulators are buck-boost, so don't think one can achieve a 3.4V output with only a 3.3V input.
I would however like to know the maximum output Vdd_x voltage value that can be achieved with a 3.3V input.
Thanks!
Kind Regards
Paul Lotter