Hello,
so i am using a customized board which contains DLP RFID2 and a CA070 microcontroller, I can successfully detect 15693 Tags. however i can't manage to detect the 14443 Tags (i am using NTAG213 and NTAG213). i tried sending the commands from the TRF7970V EVM GUI and this is what i got:
14:11:56.822 --> 0108000304FF0000
14:11:56.955 <-- 0108000304FF0000
TRF7970A EVM
14:12:18.384 --> 010A0003041001210000
14:12:18.512 <-- 010A0003041001210000
Register write request.
14:12:30.806 --> 010C00030410002101090000
14:12:30.943 <-- 010C00030410002101090000
Register write request.
14:12:43.629 --> 0109000304F0000000
14:12:43.771 <-- 0109000304F0000000
14:12:56.598 --> 0109000304F1FF0000
14:12:56.738 <-- 0109000304F1FF0000
14:13:10.848 --> 0109000304A0010000
14:13:10.994 <-- 0109000304A0010000
14443A REQA.
Does anyone of you have an idea how to be able to detect the 14443 A tags? I've been looking for a response for days now, so please help!