Hello,
I have been evaluating the RF430FRL152H using the Evaluation Board, And have been successful using an analog sensor connected on ADC0 and reading just using an Android App we built just by NFC. Now we're on the implementation phase, and I have a couple questions:
- When purchasing the RF430FRL152H. Does it come ready from factory ready to use with NFC? We designed the antenna and put all the required passive elements.
- If I connect another analog sensor to (let's say) ADC1. Are the values measured and written on the FRAM block 9 (relatively) synchronized?
- Is it possible to use a digital sensor (through I2C) just with power from the NFC field?
Thanks