Other Parts Discussed in Thread: CC1350
Hi Experts,
Now i am trying to send/receive string between two cc1350 launch pads, so i decided to convert string to ASCII value then i add to the ascii value to the rf packets i have a some doubts to do that above string transmissions
1. I am working with rfWsnConcentratorOadServer_CC1350_LAUNCHXL_tirtos_ccs and rfWsnNodeIntFlashOadClient_CC1350_LAUNCHXL_tirtos_ccs, this example transmit ADC value only but the node have a another one function
static void sendDmPacket(struct DualModeSensorPacket sensorPacket, uint8_t maxNumberOfRetries, uint32_t ackTimeoutMs)
i don't know how to enable this function and how to transmit ADC,Batt Volt,and time in milli sec
2. What is the RF packet max length and where can change the length,
3. For a example the RF packet max length is 255, so how much length string can transmit/receive 255 or 127 if 255(ascii max val is 127 so 8bit is enough) how can i do that on node and concentrator ends.
4. how can i add serial read function to node because i am trying to transmit the string which is received from serial.
i hope you understand my doubts
regards
surya