Hi there,
I recently did a range test with 2 CC1352R1 Launchpad.
I followed the steps shown in this video: https://youtu.be/mR17rNuwxrk
I figured out that the transmission frequency used in these sample projects is 868 MHz by modifying the sample project, adding extra info from the function EasyLink_getFrequency().
And also got the info that LAUNCHXL-CC1352R1 has a built-in PCB antenna already from this article: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/939167/launchxl-cc1352r1-sub-1-ghz-antenna/3468398#3468398
I had 2 laptops connect to the 2 launchpads respectively, monitoring data from the 2 launchpads through the serial ports.
And I found out the transmission distance was only like 4 ~ 8 meters. I was quite surprised by how short it was.
Do you know which parts I did wrong?