Hey,
I am working with the collector and sensor examples to establish a start network. I have a few doubts regarding the code structure.
1. Which file and what variable can I change to change my working frequencies (915MHz or 433 MHz)
2. To send the transmit data payload in which file do I set the data that needs to be transmitted by the sensor modules
3. If i want the sensor module to transmit data continuously and not at a certain interval, how can I do that?
Thanks,
Oindrila