Hello,
im confused with the LBT implementation. The problem i have is, that the random part is always the same, the time is constantly 5ms after an jammer on the air is gone.
The following settings in accordance to the LBT algorithm and RSSI are made:
CC120X_SYNC_CFG0 = 0x03
CC120X_SYNC_CFG1 = 0x40
CC120X_AGC_CFG1 = 0x11
CC120X_AGC_CFG0 = 0x94
CC120X_AGC_GAIN_ADJUST = 0x9D
CC120X_AGC_REF = 0x25
CC120X_AGC_CS_THR = 0xA2
CC120X_PKT_CFG2 = 0x10
CC120X_RNDGEN = 0xFF
CC120X_IOCFG3 = 0x4F
CC120X_IOCFG2 = 0x59
As you can see:
green = CCA Status by IOCFG3
yellow = PA by IOCFG2
What am i doing wrong here?
Thanks in advance.