Other Parts Discussed in Thread: ENERGYTRACE
I am using the example program - CC1352P-2 Launchpad/TI Drivers/rfPacketTx/CCS Compiler/rfPacketTx.
The line RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx,RF_PriorityNormal, NULL, 0);
transmits the packet and this method is implemented in the TI driver. This method takes around 15ms to transmit 60 bytes @ 450 MHz, GFSK 25kHz dev, 128kbps data rate and 10ms to transmit 60 bytes @ 450 MHz, GFSK 25kHz dev, 200kbps data rate, the maximum possible.
Additionally, the method RF_runCmd is blocking. Is there any way to execute RF_runCmd faster? Any alternative method is available for this to speed up the process?