Is it possible to use a balance antenna with the CC1101 ? how ?
There is a lot of documentation about connecting the cc1101 to a unbalanced antenna through a balun , but there is no documentation on how to connect a balanced antenna.
I have designed a balanced antenna for the ISM Band (433.05 MHz 434.79 MHz) and tried connected it directly, total failure.
Then I tried match the cc1101 with the antenna with differential network, the cc1101 has an impedance of 116 + j41 @ 433Mhz (sourde datasheet), the matching network result in something like this:
Also failed.
BUT, the same antenna through a balun (0433BM15A0001), works perfectly.
Any ideas on how can I remove the balun ? is that even possible ?
Thanks