Howdy TI and fans. Hope all are well and safe!
I am currently using an EBYTE-E70: 868 T30S. This module makes use of the CC1310.
I am doing custom development from the ground up.
I am desperately looking for the required config files (.ccfg, Overrides etc. etc.) for this module.
I have been through this manual without any luck:
The only change I have made thus far is, which does give better power consumption during sleep.
//#####################################
// Clock settings
//#####################################
#ifndef SET_CCFG_MODE_CONF_SCLK_LF_OPTION
// #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x0 // LF clock derived from High Frequency XOSC
// #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x1 // External LF clock
//#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC
#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x3 // LF RCOSC
#endif
Please can someone advise where I can find the rest of the configuration:)
Regards
Chris