I made a basic header and source file. The source file calls the header with #include "i2cBackbone.h" and contains a sample, basic method that is also declared in the header file. However when I build, I get this error:
gmake: *** No rule to make target '../i2cBackbone.c ../i2cBackbone.h', needed by 'i2cBackbone.o'.
What I'm confused is that this program builds successfully when I clean the project and I can step through, but when I build without cleaning (clean then build then build again), I get the above error. My debugger mode is in Debug and not Debug_TI(1) or Debug_TI(2). What could be a cause?