Hey guys,
we have a really tough time due to some "precise" inquires from a TCB (technical certification buddy) guy during final FCC approvement. Our network hops on 60 channels based on the 915 MHz frequency band. The channels are 67 - 126 with a dwell time of 250ms. We have already provided information from HERE and this whitepaper to the TCB guy. However, without success.
His request is as follows:
"The manufacturer need to provide a pseudo-random hopping sequence. The diagramm provided of the different nodes is not enough. They need to provide a hopping sequence of the 60 channels. This should be obtained from the software of the transmitter after a hopping sequence if possible."
I think the easiest way would be to print one hopping sequence of the 60 channels and write these values into a table for visualization of the hopping sequence. As far as I understand, this "channel timetable" is transmitted from collector to sensor within the PA frame, however, looking into the code I didnt find a way how to access this timetable and print it via the seriel interface of an CC1352R1-Launchpad. Looks like everything is happening within the stack on both sides.
Could you provide me with a hopping sequence of the channels 67 - 126 with a dwell time of 250ms from one of your boards? Or can you tell me how I can get such a hopping sequence by myself?
Please note that this is an urgent matter since our distributor in the US and canada are waiting for the approval in order to receive our sensors and gateways as soon as possible.
Best wishes
Slev1n