Hi.
I need help to calculate CC1352 board SNR. I need to estimate N0 , but some information is missing from the datasheet.
ITU-R document SM.1235-0 has several graphs for determining the Eb/N0 ratio, but does not have a graph for BPSK or 2-GFSK.
References used: ITU-R SM.1235-0, IEEE P802.15-10-0808-00 and Sklar (88).
Do you apply another method for SNR?
Formula: C/N = Eb/N0* fb/Bw
Eb/N0 = 11,1dB
fb = is the bit rate, and
Bw is the receiver noise bandwith
Eb/N0 : was taken from a graph BER vs. Eb/N0 from Intersil.
Thanks.
Rafael Minhoto.