Other Parts Discussed in Thread: UNIFLASH
Hi it appears my launchpad is not detected by uniflash anymore... the firmware still seems to be running though, (the led set by the firmware is on). I tried a coupled things, restart uniflash, re-download uniflash, restart computer, checking that the usb port was not broken by using other usb devices on it and pugling the board on another usb port. I also checked if the board was detected at all by the computer, I ran lsusb the device was not appearing in the output, I also checked if the device file i.e. /dev/ttyAM0 was here, but it wasn't. Couple of precisions : I am on a linux system, and I do not use Code Composer studio IDE I only use uniflash to flash the firmware and reset the flash.