Having previously successfully built a project in CCS from Sensor Controller Studio, no getting this error:
static int scifFindLeastSignificant1(uint32_t x) {
#if defined(__IAR_SYSTEMS_ICC__) || defined(DOXYGEN)
return __CLZ(__RBIT(x));
#elif defined(__TI_COMPILER_VERSION__) || defined(__CC_ARM)
return __clz(__rbit(x));
#else
return __builtin_ctz(x);
#endif
} // scifFindLeastSignificant1
error 1- can't resolve _clz
error 2 - can't resolve _rbit
I have re-installed Sensor Controller Studio , where are the aboves defined?