I'm experimenting with a pair of LaunchPads running the collector and sensor demos. For real world use, I want the collector to automatically start the network on power up (which can be done using CONFIG_AUTO_START), but would also like it to automatically allow sensors to join the network. Likewise, I want the sensors to power up and immediately join the network. What are the necessary and sufficient steps to accomplish this? I haven't been able to tell from the documentation when it would be safe to call Csf_openNwk() on the collector side, for example.
Thanks!