Other Parts Discussed in Thread: CC1310, SYSBIOS
Hi
I work with IAR (not CCS) on porting Project on CC1310 to CC1312.
IAR: 8.50.1
SDK: simplelink_cc13x2_26x2_sdk_4_40_04_04
I started with an example project
then I made changes to work with my project.
I had issue with the .cfg so I replaced the original one.
Instead of Release.cfg , I replaced it with a new file: Modem_CC1312R1.cfg that contain my things and it compiled well.
Recently, I had to reinstall the environment.
I uninstalled the SDK & IAR and installed them again.
1) The Compiler gave me this:
Error[Li005]: no definition for "ti_sysbios_gates_GateAll_enter__E" [referenced from C:\P4Client\Workspace\CC1312_RFD\RF\PersonalBranches\YigalBu\CC13xx_Platform\_source\application\modems\_project_CC1312\Debug\Obj\powerCtrl.o]
I got it in the past and fixed it by replacing the .cfg (as I mentioned before)
So maybe it ignore the .cfg file. I tried to remove it from project and add it again. no change
Any ideas?
2) After uninstall and install IAR it still remembers the last project. I wish it was clen (no history)
Any ideas?
I'll appreciate your help
Thanks
Eyal Chen